Hi
I am using drv201 +mux in our product in order to activate some kind of motor.
with the drv201 we generates 10 HZ signal - ( absolute - sin or rect) and with the mux we do it positive or negative so the signal will be regular sinus or rectangular wave.
our motor has ~630uH inductance and 100 ohm resistance and it is working with the drv201(olthough it is out of spect)
in order to approve our product I would like to activate the our motor using DRV2605 wich I saw can generate positive and negative voltages.
my question can in produce 5-15 Hz sin continually?
what are the inductance and resistance limits of the motor? I havet seen in *** spect.
If this is driver is not good for such motor can you please advice how else can we do it?
thanks in advanced,