I have 2 signals between -1,1 and -30,30. The frequency of the signal is 2 and 5 Mhz. I would like to use OPA365 combined with tms320f2811. What is the best way to change the gain of the amplifier?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have 2 signals between -1,1 and -30,30. The frequency of the signal is 2 and 5 Mhz. I would like to use OPA365 combined with tms320f2811. What is the best way to change the gain of the amplifier?
Hi Robert,
The TMS320 has multiple ADC inputs, so you can set up a channel for each input signal. The OPA365 has an absolute maximum supply voltage of 5.5V, so a passive attenuator will be required for the -30V to 30V signal. If you set up the attenuator to attenuate the +-30V signal to +-1V you can use the same gain for both signals.
Loren