Hello,
Can I have the following data of THS3001?
(1) input offset voltage drift (max)
(2) distribution data of input offset voltage drift
Best Regards,
Ryuji
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ryuji,
I searched for the data and cannot seem to find the raw data, however I have found the statistical data for each of the temperature extremes and nominal. Please see below, this is the Vos in uV @ +/-15V supplies
Temp | #Samples | Smpl Min | -6 Sigma | MEAN | +6 Sigma | Smpl Max | Sigma |
-40 | 67 | -1055.15 | -1642.53 | -716.393 | 209.748 | -376.428 | 154.357 |
25 | 74 | -1191.12 | -1769.03 | -880.083 | 8.863 | -551.577 | 148.158 |
85 | 73 | -1519.94 | -2214.97 | -1168.3 | -121.626 | -793.117 | 174.446 |
I will continue to search for the raw data so that we can extract more meaningful drift data.
Samir
Hello Ryuji san,
Looking through the Vos data the part looks well behaved across temperature. The sigmas and data range look consistent across temperature which gives me confidence that the mean Vos drift can be calculated just as you have calculated above. The same goes for the min and max "samples". However, looking through the data I dont think I can make any conclusions on the Sigma of Vos drift.If I assume that the mean, max and min vos drift are from three individual units I feel very strongly that the drift of the part is very well behaved.
I discussed this with some of the statistical gurus here and their conclusion is the same. We however dont agree with your calculation of the Sigma of Vos drift above. Hope this helps.
I got in touch with product engineering and we cant seem to find the data on the individual units. This is a very old part (1999) and we are not sure who the engineer working on it at the time was.
Samir