Hello all,
I want to make my first transimpedence amplifier using opa380, the circuit as shown if the figure no. 1 of datasheet with BPW34 photodiode from vishay. But the problem is that I get no variation in output if I illuminate photodiode. The output remains constant at 5V only. The photodiode is working as i tested it using it in series with a resistor and measuring voltage drops. I want arround 3 MHz bandwidth. But currently I am testing the output by just turning on and off the light on photodiode. Is it ok to do so ? Will I get change in output ?
What can be possible reasons for this ?
I am using 1M feedback resistance.