Hi Hooman,
This is in continuation of my previous post on difficulty in observing the main o/p of LMH6518 on oscilloscope, while aux. o/p was coming correctly. I have replaced the part as you advised and now getting the main o/p. But now I am getting low amplitude at the aux. o/p. The aux. o/ps are connected like fig.-68 of data-sheet.
The single ended aux. o/p is 140 mV(pp) riding over a 1.2V CM, the differential aux. o/p is 264 mV(pp) while the diff. main o/p is 480 mV(pp).
All the differential o/ps were measured using a differential probe and all single ended o/ps were measured using a 10X probe terminated at 1MOhm.
Please help.
Regards,
Supratim