Hello everyone,
first a disclaimer, I am a mechanical engineer. As a grad student, I need to build an AC amplifier with current limiting (and it needs to function for my experiments for the next year or two). There is a nice Burr-Brown application note on this subject here http://www.ti.com/lit/an/sboa042/sboa042.pdf figure 2.
My challenge is that I'd like this beast to operate at up to 10MHz (higher if possible), +/-5V. The signal is a pure sinusoidal tone. There is a note about stability on page 1, column 2 and I am having a heck of a time finding an op-amp to use in place of OPA2277 that has a slew rate >100V/microsec and bandwidth that is greater than 20MHz. Does anyone know, can I use a faster op-amp, like an LM6172 and add an RC "filter" to the feedback loop around A2 and A3? Do I need to worry about stability if my signal is just a single frequency sinusoid. Alternatively, could I just add gain to the A2 part to slow it down? My signal comes from a function generator so I am pretty flexible on the input side.
While I'm at it, I need a higher current output than a single BUF634 can provide. I'm planning to try driving 3 of them in parallel and I know that voltage mismatch at the outputs can cause problems for regular op-amps. Can I tie all 3 buffer outputs together before the sense resistor or should I use a resistor for each one and tie them together afterwards? Or do I have to build 3 entirely separate circuits altogether and tie them at the output? There is not much power going through the first two stages but I am not sure how to handle the feedback circuitry.
Someone, help out a Mech E! Thanks!