Hello,
I am having difficulty with noisy outputs from this simple circuit below, that I built on a breadboard. It consists of two inverting op amps; the first has gain of -2, and the second has a gain of -1, so the total gain is (-2) x (-1) = 2:
The signal on the scope looks good when probing the red dot:
But at the final output (blue dot), I get this:
The op amps are powered at +/- 20 V.
Any idea why the second input is so noisy? The noise does not depend on frequency or amplitude of the signal.
Thanks much,
Aaron