Dear TI Support,
I am looking for a fully differential Amplifier to convert bipolar (+/-2.5V) signal from a current sensor (2MHz bandwidth) to differential signal to a 65MHz TI ADC. I found THS4121 and THS4531 could do it. But I am not sure about the pull-up resistor circuit to the power supply. In THS4121 datasheet, it recommends using pull-up resistor to limit the common mode input voltage to V+/V-, as the the sensor's output might be higher than the nominal output 2.5V. Is that circuit applicable to all the fully differential amplifiers (incl. THS4531)?
Tahnks