Hey All,
I'm planning to use the LMH6629 with an multi-turn coil antenna around 30~300 kHz, but I am undecided between using it in the inverting or the non-inverting configuration, and how to achieve the best SNR. Below are my thoughts, please feel free to correct me if I'm wrong.
1. In the Inverting mode, the input impedance of the op amp will be the input resistor Rg, where Av = -Rf/Rg. Rg is easily matched to the real part of the coil antenna. Although power matched, it may not be noise matched.
2. In the non-inverting mode, I think the antenna can generate a lot more voltage at the non-inverting input, or just have it unterminated, to minimize the NF.
3. Incorporate a 1:4 turn transformer such as the http://www.minicircuits.com/pdfs/T36-1.pdf to further boost the NF.
Let me know your thoughts
Thanks,
Albert