I would like to use the LMH3401 in a single supply (5V) application where the input signal will swing around 0V. In the electrical characteristics section, page 6, it says:
Input common-mode range low: typ VS- - 0.7 V, max VS- + 0.2 V
This seems to indicate that 0V common mode might not always work well for all LMH3401. But on page 22 it says:
"The input common-mode range extends from the negative rail to approximately 1 V above the mid-supply voltage when powered with a 5-V supply."
So, can I trust that I will not severely degrade distortion performance if I use the amplifier with a common mode input level of VS-?