hello,
I need to amplify a 4MHz signal with an amplitude of 10mV so that the output varies between 0 to nearly 5 volts. This signal lasts for about 5 micro seconds.I wish to amplify it using a single stage amplifier with single power supply of +5V. My current solution is to use two OPA354 amplifiers. It seems to work in TINA-TI, however if possible I would like to do the same with a single amplifier.
Can any one please suggest an amplifier that can achieve this task?
Best regards,
Umar Khan