Hello Ti community ,
I am evaluating lmh3401 for RF applications, please someone can provide me the S-parameter? maybe, if possible in differential in to differential out condition?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Matteo,
Here are S parameters with a 37.5 Ohm input resistor to match the inputs to 100 Ohms differential as well as 40 Ohm output resistors to match the output to 100 Ohms differential. This is tab delimited text, so to open it in Excel you need to open it and select "delimited" and check the "tab" box.
You can get the actual impedances by subtracting 75 Ohms from the input impedance numbers (Sdd11) and by subtracting 80 Ohms from the output impedance numbers (Sdd22).
Regards,
Loren