Hello ,
I am using lmh6881 for a certain project , my question is i have another differential(THS4500) before lmh6881 that outputs a differential signal output with DC offset Voltage at 2.5V. On datasheet(page 19) it states that it is possible to externally bias inputs to 2.5 , therefore will it make sense as a design point of view to directly input this differential signals to the DVGA (Lmh6881)? Also if i do that the datasheet also states that it is internally biased to 2.5V will that make DC offset at 5V and cause the DVGA to malfunction?
I would greatly appreciate any help on this ,
Thank you.
Regards