Hallo,
I have added simulation results.....
I have done a Tina simulation with a THS 4521. (Gain 1V/V; with 4pcs of 1k resistors; both Inputs are AC decoupled with 100n caps; single ended input signal 500mV: 5V supply voltage; Vocm=2,5V; output differently loaded with 1k. )
I have done the AC transfer characteristic from 10MHz to 100MHz and i got on the + output a frequ response -6dB to -7dB....if I measure at the - output I get a frequ. response from -6 to -10dB.
What is the reason for this 3dB difference between the output channels and why is the inverting output not so flat like the non inverting output.
kind regards
Rudi