Hello TI community,
I am looking into an application for LMH3401. I have downloaded Tina9 model and test schematics for the device, but I am having trouble with PD pin.
The original schematics (SBOS695) uses a complicated auto-centering two-rail power supply arrangement, but with negative rail set to zero, and positive to +5V.
When I simplified the power rails to plain +-2.5V, the question was how to connect the PD pin to enable amplification.
The datasheet for LMH3401 says that if the PD is "High (> GND + 1.2 V) = low-power (sleep) mode. Low (< GND + 0.9 V) = active."
However connecting PD to GND results in attenuated signal and apparently inactive circuit.
I noticed that the PD is referenced to VEE (= Vs-) in the reference schematics. If I connect the PD to VS-, the circuit works.
The question: is this an error in the LMH3401 model, or is it a misprint in documentation?
Thanks.