Hi there,
trying to implement the VCA810 in a customer application we found some odd things.
- Page 3: voltage output swing contains two entries with the same text “Vc = -2V, RL = 100Ohm”
-> what is the difference and why?
- Page 5: Input offset current is far beyond reasonable values: 700mA max. (!)
-> it should be magnitudes lower (nA instead of mA ?)
Thanks for a quick answer
-Bernd