Hi,
I need the ESD rating, MSL rating and terminal finish for part number BUF634FKTTT. This is not listed on the datasheet.
Thanks,
David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I need the ESD rating, MSL rating and terminal finish for part number BUF634FKTTT. This is not listed on the datasheet.
Thanks,
David
what is the JEDEC standard classification? I need an MSL rating such as 1,2, or 3.
Separately from this table, I also need the terminal finish. Is it pure tin? NiPdAu?
Regards,
David
Hello David,
Here is the requested data:
MSL - Level 3 @ 260C peak
ESD - HBM 500V
Terminal Finish/Lead Finish: Matte Tin, 100% Pure Tin