en |
Noise voltage |
Input referred f > 1MHz |
0.69 |
nV/√Hz |
||
in |
Noise current |
2.6 |
pA/√Hz |
|||
NF |
Noise figure |
RS = RT = 50 Ω |
8.0 |
dB |
Above numbers are from the LMH 6629 datasheet.
I am just trying to calculate the noise figure and arrive to the same NF number published in the datasheet.
It seems like I should be able to combine the input-referred voltage and current noise, given a 50-Ohm source, to come up with a total input-referred voltage noise. And I ought to be able to then calculate the amplifier’s noise figure. However, my numbers don’t seem to work out when I attempt this.
Per my calculations, the total input-referred voltage noise comes to 0.7nV/Rt Hz
Then I use this formula:
NF = 10log(1+NA/Ni)
For NA is use the calculated input-referred voltage value of 0.7 and for Ni I use 0.91 nV/RtHz (50 Ohm source thermal noise)
Thank you in advance for the help.