HI ALL,
I am using a FDA (THS4151ID) as Av = 1/5= Rf/Rin amplifier configuration with digital pots (AD5293) as Rf and fixed resistors (5Kohm) as Rin. Load to this FDA is an ADC (ADS850) +in and -in terminals. FDA HAS 25ohm resistors and filters (S3LP156L) at both output nodes, before ADC . I have also provided an extra digital pot Rt (AD5293) between inverting and non-inverting terminals of FDA to compensate for NOISE gain 2. Removing and placing of Rt makes no difference on heating problem. EVEN I HAVE TRIED TO PUT CALCULATED VALUES FOR Rt as per formula given for FDA noise gain stabilization under heading "Using an FDA’s RF and RG as an attenuator " in the mentioned document below. input to this amplifier is a bipolar differential 20 Vpp signal.