This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6881 Power ON Status at Serial Mode

Other Parts Discussed in Thread: LMH6881

Dear Sir,

LMH6881 sometimes keeps Amp Power Off situation after Vcc powering up under Serial Mode (SPI Compatible) until writing Register 2 to power on.

Pin connections are as follows;

SPI pin : directly connected to Vcc

SDO(D0) pin : Open

SDI(D1) pin : Lo level input  / FPGA

CLK(D2) pin : Lo level input  / FPGA

CS(D3) pin : Lo level input / FPGA 

SD pin : connect to GND through 270ohm

As SDO is open (not use read-back by FPGA), then I could not check Register 2 status when the device was power-up.  

Questions are;

- Isn't LMH6881 always power on status at powering up under serial mode?

- Abut pin connections, especially above SPI, SDO, SD connections are okay? Is there any suggested connections including unused even disable pin like SD? SPI pin becomes Vcc from zero volt at powering up. 

I understand default Register 2 is power ON(0,0) and SD pin is disabled at serial mode.

I expect that the device is always power on status just after powering up at the serial mode.

Best regards,

Masa