Hi,
My customer wants to using THS6182 in G3 PLC for power line driver. Their system requires the driver has capability to drive 20ohm to 20Vpp. Such the amplifier should be able to deliver 1A output with 20Vpp output swing. While THS6182 can only deliver 600mA. To meet this requirement, I am considering recommend them using two amplifier (in same package) in parallel with master-slave topology. I am not sure if this amplifier can be used in this topology? is there any potential issue?
Thank you,
John