I have 10X gain mode enable on ADC Pi Plus. This requires the full-scale ADC range, FA, to be limited to 625 mV otherwise this ADC can be damaged. The full-scale signal range, FS, from the sensor normally should not exceed 525 mV but worst case it could exceed 625 mV. To summarize the ADC Counts: C = FS/(FA x 1/g) x 2^N, where N = 16 bit resolution and g =10, the programmed gain option via software API.
Q1. Per the Single Supply, Limiting ADC Input Driver circuit shown in TI OPA698 Figure 5 Page 16, is the correct solution for my application to simply substitute a voltage divider yielding 525 mV that is applied pin 8 and pin 5 is tied to ground?
Q2. Unity gain is desired. Is it acceptable to tie inverting pin 2 to output pin 6 and apply sensor input signal directly to non-inverting pin 3? To contrast, the circuit shown in TI OPA698 Figure 5 Page 16 has two 715 ohm resistors pin 3 and two 402 ohm resistor feedback from pin 6 to pin 2. Can these extra resistors be ignored? If not, what's their purpose with respect to the OPA698 ensuring voltages greater than 525 mV are limited?
Thank you.
~ Mike
References
[1] Sngle ended full-scale range of 5.0V ADC operating in10X gain mode, https://www.abelectronics.co.uk/p/56/ADC-Pi-Plus---Raspberry-Pi-Analogue-to-Digital-converter
[2] FIGURE 5. Single Supply, Limiting ADC Input Driver