Hi,
I have some questions on THS7530 and need some help.
1. In the datasheet, in Figure 21 DC-Coupled Single-Ended Input With DC-Coupled Differential Output, there is a 0.1uF capacitor behind the Vin input, how can this be a "DC-Coupled Input" ?
2. In, Figure 3. Noise Figure vs Frequency, NF=30 for Gain=20dB. Does it mean if I use a signal source with SNR=30dB, after the 20dB amplification, the SNR of the output signal is 0dB?
3. How to use the Total input voltage noise to calculate the noise at the output? For 300MHz bandwidth, the total input noise is only 20uV. If the input signal is 0.6mV with 20uV noise (SNR=30dB), after Gain=20dB amplification, the signal is 6mV, and the total noise is (0.02+0.02)*10=0.4mV. So the output SNR=20log(6/0.4)=23.5dB. How can that be the 0dB calculated using the noise figure?
4. I use the TI TINA and the provided simulation model to calculate the output noise. With 10mV input, the 300MHz total noise is always around 5mV, despite setting of gain. So it is different from the value calculated with the total input voltage noise or the noise figure.
Thank you in advance.