Dear Sir/Madam,
I am looking at using the LMH6553 to interface to an ADC because of the clamp feature.
The ADC input has 27K from each input to ground and 5.8pF from each input to ground.
The ADC common mode input is 2.0V and input min/max is 1.3V to 3.0V.
The LMH6553 would be connected single ended and driven from an VFB op amp.
I would like to use a 40MHz RC low pass filter between the
LMH6553 and the ADC. The application requires a flat frequency response (no peaking) for the pulse input.
The datasheet shows peaking with large load resistance. Does this seem possible?
Regards Grant