Hi,
I am using OPA2354 for detecting the peak of 180KHz pulses at 1.8V.
As I don't want to interfere with input or output impedance, I am using input buffer and output buffer as shown in below schematics with a diode in the input buffer feedback stage. VCC is 5V.
I have a basic question that this OpAmp is suitable for this requirement? And the output of the output stage will be of 1.8V?
Thanks & BR,
Pradeep.