This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bootstrapping a photodiode

Other Parts Discussed in Thread: LM6171, LMC6082

Hi,

I'm trying to design the first stage (transimpedance amplifier) of a radation detector with a "common" photodiode.

Sytem details:

The goal of the first stage is to have a pulse when some kind of radiation impact the photodiode. This will produce a 15/20 nA - 50 us pulse.
Photodiode: Vishay BPW34 (70 pF - 2 nA dark current in photovoltaic mode (0V bias))
Necessary bandwidth: 20 kHz.

The transimpedance amplifier seems to be ok with low frecuencies. I've simulated a 3 photodiode array with C1 (capacitance = 210 pF), IS1 (dark current = 6 nA) and IG1 (a 15 nA - 50 us pulse).

Naturally, the capacitance of the photodiode begins to cause problems with frequency. As is indicated in most technical literature, the photodiode can be bootstrap with a voltage follower, improving the bandwidth. But when I've tried it I begin to have problems.

This is, for example, the AC gain with a LM6171 as voltage follower:

What I'm doing wrong?

Thanks!Transimpedancia 01.TSC