This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
This application note briefly discusses the difference between the Voltage Feedback (VFB) and Current Feedback (CFB) type Fully Differential Amplifiers (FDA) in terms of their differential input impedances, on pages 3-4 . The LMH6552 is of the CFB type:
"In a VFB FDA, the differential input impedance is very high (usually hundreds of KΩ to several MΩ), and ..."
"A very different result arises when a CFB FDA, such as the LMH6552, is considered. Here, the differential input stage is essentially a current controlled current source, with ideally zero differential input impedance...."
With the LMH6552 operating in closed loop, there will be a "virtual short" across the differential inputs (similar to the idea of "virtual ground" in the more traditional op amp terminology). That is, the feedback ensures that the two inputs are at identical potential (except transient behavior when the loop is trying to servo the two inputs together). Thus, there is no steady state voltage differential and subsequent current flow with either VFB or CFB type FDA's.
Regards,
Hooman