I’m trying to simulate an LMH5401 and I’m using the circuit from app note tiduba4 as well as the datasheet. I don’t get your results at all.
If you plug in numbers into the gain equations for the LMH5401 the resulting gain does not equal the simulation. I’m using TINA and TI’s SPICE models. If I SPICE their oscilloscope circuit, I don’t get any gain at all. I only get attenuation. If the input is 0.25V and the input divider action cuts it in half, which you would expect for a matched source and load, the output is then something like 40mVpp. The positive output might be a volt but the negative output is also almost a volt. This is for the LMH5401.
I can also get results that work with the LMH5401 but I have to use feedback resistors of 2K-Ohms in order to get a gain of 12V/V. I have a small input resistor, like 36 Ohms and a feedback of 2K-Ohms. I am negatively biasing the positive input and feeding the input into the negative input. My signal only goes negative from 0 to negative 0.25 or -1 or -4.
I need to know how biasing the input shows up in the output.. You claim that setting the bias voltage to half the input signal range will cause a bipolar output. I agree with this and I can simulate this but the voltage is never half the input swing. It’s always somewhere else. I can’t figure out why there’s a difference between what youand I would expect and the simulation.
I’ve attached a simulation file. Could you please help me to figure this out?
The other issue is input impedance. I can calculate and simulate and get agreement on input impedance because I see the voltage get divided in half when I match the amplifier input to the source impedance. However, again, this happens not by calculation agreement but more by trial and error with huge gains.
Thanks and Best Regards,
-Tim Starr on behalf of GG@ESLMH5401-VS2.TSC