您好,我初次用lmp8672,给的输入信号是5MHz,5V的方波信号,供电是正负12V,为什么没有输出呢?请问这款芯片的做放大器时的参考电路是什么样的?RF和RG的取值关系如何?这些官方网站提供的datasheet上没有应用的示例。请技术支持给与帮助帮忙解决一下,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ai,
I used Google translate to make your question english. I hope it is a good translation.
"Hello, I first use lmp8672, the input signal is a square wave signal to 5MHz, 5V, and the positive and negative power supply is 12V, why did not export it? Will make a reference amplifier circuit chip is what? How to value the relationship between RF and RG? There is no example of an application on the official website of the datasheet. Please help to give technical support to help solve what, thank you!"
Can you post a schematic? What gain and amplitude are you using?
If you look at Figure 19 in the datasheet you can see that a 1Vpp signal of 5MHz is hitting the bandwidth limit of the amplifier. Larger signal and square wave won't work, you will need a faster amplifier or a smaller signal.
This part is in the precision product line, not the high speed. I will move the post into the precision forum and maybe they can provide more information.
Regards,
Loren
Hello Loren,
First ,I am very sorry that I didn't answer in time,and then, thank you for your prompt reply.I have looked the THS6022.Comparing to LMP8672,THS6022 is a better choice.But there is a problem that I need a part which could output a 5MHz ,at least 40-V p-p signal.Although there is a description of "These drivers can be configured differentially to drive a 50-V p-p output signal over low-impedance lines" in THS6022's datasheet , but I don't find how to do.
I would be grateful if you could give me some advice.
Thank you very much!