Hello there,
Can I use an OPA695 as a differential-to-single-ended DAC output amplifier instead of THS3215?
Many thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
That is certainly possible as long as it meets your output swing and distortion specifications. You will also lose the ease of the integration capabilities of the THS3215/THS3217.
Do you have a particular reason for choosing the OPA695 over the THS3215/THS3217?
The application note below shows how to use the OPA695 in a DAC differential to single-ended application.
Hi Samir,
Thank you very much for your reply.
I believe that OPA695 is faster, cheaper and smaller.
Kind regards,
Bailin
Hello Bailin,
I have a couple of suggestions/inputs:
1. Using the D2S to drive a 50 ohm load - You are actually driving a total load of 100 ohms with 6dB of attenuation (50 ohm match). The D2S can drive a 100 ohm load without significant degradation in bandwidth (see Figure 14 of datasheet). From my experience the distortion of the D2S degrades by only 2-3dB under 100 ohm vs 200 ohm load.
2. Using the full signal path, i.e OPS + D2S - I believe you can actually do this and get your required gain. I would recommend adding a filter stage between the D2S and OPS (as shown in Figure 95).The interstage filter in figure 95 has a low insertion loss, but you can add more insertion loss by changing the value of the 464 ohm and 90.0 ohm resistors. Are you using a DAC to drive the amplifier? In that case you can maintain a full signal path gain of 5V/V and just reduce the DACs dynamic range.
We have a system level design of a DAC + THS3217 to help designers simplify/accelerate their design process. In case you are interested you can find the information here.
-Samir