First post to E2E.
I have a design that utilizes several NE5532 opamps in a simple voltage follower configuration. The amps are intended to buffer a balanced audio signal, and each amplifier is connected to four similar buffers. While the circuit performs well and the current draw appears normal, the parts seem to run quite a bit warmer than I would expect. I am operating them on +/-15V power supply rails (bypassed with 100nF) with each amplifier drawing 7mA per rail. I have measured the temperature of the device case (SO8) at 50deg C. I believe this to be within recommended operating spec but am concerned about long term reliability. Below is the circuit.