Hi,
In one of my Applications, using OPA2836IRUNT (1st channel) as a Differential to Signal Ended Amplifier with gain of 20, Rf= 10K, RG= 0.5K with 0.01% tolerance.
I'm not seeing an expected output rather than getting Vout= Vout +/- 10mV if I use Rf with 0.01% tolerance. But, when I relax the tolerance to 0.5%, I am able to get the expected output without any error.
Could anyone help me what makes the difference in operation of these cases briefly?