I am trying to calculate the offset error (referenced to the input) due to common mode voltage on the power rails for a dual rail device.  I know it is simply the common mode voltage divided by the psrr which is stated in the datasheet.  However, what is the common mode voltage?  If the positive voltage is +15V and the negative is -14V is the common mode voltage 15-14=1V or is it 14V or some other value?