Other Parts Discussed in Thread: LMH5401
To Whom it may concern:
Can the LMH3401 be used as 2GHz TIA with inputs from 4.5nA to 500nA?
Thanks
Art
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Art,
The LMH3401 has on chip Rf and Rg resistors, it cannot be configured as a TIA. The LMH5401 is built on the same core and has no on chip gain set resistors. I have configured the LMH5401 as a TIA with good success using a photo diode. I get around 1GHz of bandwidth with the diode I used. The bandwidth of my circuit was limited by the diode capacitance. You will need to have a very small amount of capacitance on the amplifier input to get 2GHz of bandwidth.
You will need to be able to extract your signal from the broadband noise. Our current noise is 3.5pA/rtHz. If you integrate this noise over 2GHz of bandwidth you get 157nA of current noise. Depending on your signal spectrum you may be able to extract it from this noise.
Regards,
Loren
LMH5401_TIA_3.TSCHi Loren!
Can the LMH5401 configured as a TIA be able to work from a single 3.3V or 5V supply. For some reason, my simulation does not work with single source supply (see attachment).
Thanks
Art