Support Path: /Product/Development and troubleshooting/
To whom it may concern:
Can you suggest the best differential OPAMPs/RF amplifier to use for amplifying the a uV to mV ( a factor of 1000, 60dB) and still have bandwidth of 2G?
Thanks
Art
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Support Path: /Product/Development and troubleshooting/
To whom it may concern:
Can you suggest the best differential OPAMPs/RF amplifier to use for amplifying the a uV to mV ( a factor of 1000, 60dB) and still have bandwidth of 2G?
Thanks
Art
Hi Art,
I would add a couple more part numbers to the mix. The first is the LMH6401. As Samir mentioned, linearity will be an issue at the higher frequencies, but with small signal amplitudes the LMH6401 may be linear enough for 2GHz operation. A benefit of the DVGA is that bandwidth is constant over the frequency range.
Is your input signal differential or single ended?
Once you start your board design it would be good to use some kind of shielding between the output and the input. With 60dB of gain and multi GHz bandwidth the circuit will be prone to feedback and oscillation. This is one benefit of multiple stages because each stage will be less likely to have feedback.
Regards,
Loren