Hello,
I'm writing regarding the PD# pin on the THS4541. In particular I'd like to drive it with a 5V push-pull source. Voltage rails of the THS4541 will be +5V and GND.
Under this circumstance if I drive the PD# pin to 5V, will the op-amp be enabled when PD# > 1.7V and disabled when PD# < 0.7V?
From my understanding of the datasheet, the answer is yes; but, I'd like confirmation.
Don