Hello,
I'm writing regarding the DIS# pin on the OPA847. In particular I'd like to drive it with a 5V push-pull source. Voltage rails of the OPA847 will be +/-5V.
Under this circumstance if I drive the DIS# pin to 5V, will the op-amp be enabled at VDIS > 3.95V and disabled when VDIS < 1.5V?
From my understanding of the datasheet, the answer is yes; but, I'd like confirmation.
Don