Hello E2E,
I need to be able to test a products video input to ensure it will tolerate a +-5V common mode voltage. This is analog video so think of an NTSC video type of signal (1.2V p-p), but it is input to the product as differential.
I selected the THS4140 fully differential amplifier since it has the OCM pin. I run the THS4140 from +-12V supplies. I connect a separate supply to the OCM pin for +-5V variation capability. I have the amplifier set for gain of 1 and have tried both 390 OHM and 1K OHM resistors for Rf and Rg (your data sheet ref des).
I use a NTSC signal generator and run the circuit as single end to differential conversion.
When I look at the output I get a nice differential version of the input over a common mode range of ~0+-3V. The output varies up and down nicely while I vary the VOCM source as expected. But as I go above +-3 V, the output starts to distort and by about 4.2V the output is completely smashed. The outputs continue to follow the OCM voltage up to 5V(where I stop), but the signal is killed off.
What am I missing? I figured as a crude estimate that 5V+1.2V is <7V and so +-12V supplies should have way more than enough "head room". I even tried running at +-14V and that didn't make any difference.
I am basically running the circuit from figure 30 of your data sheet, with an additional 75Ohm termination resistor to ground across the input signal source. I dont see the input source begin affected other than the smaller Rf and Rg values tended to "pull it up or down" slightly.
So I need some help getting this running to the full +-5V without distorting the output. Also out of time for my test phase.
Thank you for the help!
Regards,
Russell