I am going to design a circuit to control the hysteresis of the comparator LMH7322 as the following circuit, but we found some comments on the datasheet page 23. It said “Connecting the RHYS pin to another voltage as provided by the RHREF pin is not covered in the resistor selection plot and the designer of such a circuit must be aware of abnormal behaviour.” My design is not connect the voltage reference to RHYS pin directly but through a 1K resistor, I hope it will not cause any abnormal behaviour. Also, how accuracy the hysteresis control can be achieved if you can give some estimation?