Other Parts Discussed in Thread: TINA-TI
Hi,
One of my customers has the below questions regarding the Transimpedance amplifers.
1) In application note SNOA942 "Transimpedance Amplifiers (TIA): Choosing the Best Amplifier for the Job", a design example for photodiode is given (section 3). They have proposed LMH6629 opamp having 15uA bias current for interfacing a photodiode having a maximum current output of 1uA. How can this be justified?
2) If I am using an opamp having GBP of 2 MHz, the maximum Transimpedance gain I can give for current to voltage conversion of a 10KHz signal is only 200 ?.
3) Once the current is converted to voltage using a TIA whether the following preamplifier bias/offset currents have strong impact on the performance of the channel.i.e.Whether using opamps having bias currents in uAmperes for amplification/filtering after the TIA (for converting uA
currents) is a good design practise.
application note SNOA942