Part Number: ONET-10G-EVM
Hello, I've got some question about the SFP+ breakout board.
I've a ZR type sfp+ and I'd like to track the receiving optic power, so I think the RSSI feature on ONET-10G_EVM would be helpful. Here are my question:
1) Is the ONET-10G-EVM LR compatible with SFP+ ZR type? which is a type sfp+ allow signal transmitting up to 80km.
2) Regarding to the rssi signal, how fast the signal can i get(frequency)? is it real time?
3) Is there any other device needed other than onet-10g-evm for my purpose? I'm going to purchase a set if necessary.
Thank you very much!