Other Parts Discussed in Thread: ADS4246
DEARS.
I want to use THS770006 and ADS4246.
Are there design issues for THS770006 and ADS4246?
Help me review the schematic.
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Henry,
Please see below for modification to the input circuit while driving the THS770006 in single-ended to differential configuration from a 50-ohm source.
If you are driving the device with a 50-ohm source, then it is not necessary to have the R342 (or make it DNP). But then, you would have to make the 25-ohms connected on the un-driven input as 50-ohms for getting a balanced impedance looking into the device inputs.
I would also make the R322 and R323 as 49.9 ohms to attenuate any charge kick-back that could occur at the amplifier outputs while sampling the inputs at the ADC.
Best Regards,
Rohit