Dears,
Customer tests op-amp THS4121 input and output, no output is detected.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Cris,
Is the customer applying a DC voltage at the input? If yes, then it is possible to not notice any signal at the output because the input is AC-coupled by the series cap C62 and C65. The other thing is that applying a +/-3mV input results in only a +/-150mV output which is a very small signal difference at the output. You might want to increase the signal to +/-15mV in-order to see any noticeable output signal.
Also, is there a reason for the customer to use 1M-ohm resistor on the feedback - R35 and R46? The output of the circuit would be too noisy with the 1M-ohm resistor. I would recommend using a reasonable value for the feedback of ~10-kohms and then scaling the Rg accordingly to 200-ohms for -50 V/V gain.
Best Regards,
Rohit