Other Parts Discussed in Thread: LMH6881
Hi
Currently using VGA as LMH6518 (below is the circuit for the same). The output of this is given as the input for the ADC LTC2191.
As per datasheet the maximum output swing at the VGA out is 0.8Vpp only. Please confirm the below queries.
1) whether it can have output voltage swing of 0V to +2V.
2) Or do we have to change the PGA to LMH6881.
3) Can it be interfaced withLTC2191 ADC directly after the coupling specified in the ADC datasheet