I'm using the LMH6654 as a comparator for a project and I was wondering how to compensate for input offset in a circuit that uses the op amp in open loop configuration. All the solutions I come across provide only closed loop solutions.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm using the LMH6654 as a comparator for a project and I was wondering how to compensate for input offset in a circuit that uses the op amp in open loop configuration. All the solutions I come across provide only closed loop solutions.
Hi Anthony,
Yes. If you place a 0.5V DC voltage on your non-inverting input, then anything above 1.7V (or -0.7V on +/-2.5V supplies) on the inverting input will possibly damage the op-amp even though the maximum input using a 5V supply is 5.5V. Or say, if the non-inverting input is at 5.5V DC, then anything below 5.5 - 1.2V = 4.3V on the inverting input might possibly conduct the differential input ESD diodes to damage the inputs.
Best Regards,
Rohit