This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI Ali,
Your problem is likely with the buffer configured amplifier that you are using. The LMH6629 requires a minimum gain of 10 V/V in its default configuration for stability. The WSON-8 package includes a compensation pin that can be driven to reduce the minimum required gain to 4 V/V at the loss of some bandwidth, which would work for your last stage.
It's a bit challenging to comment on the stability of your transimpedance stage because it looks like you are trying to "bootstrap" the capacitance of the diode which will have some effect on the amplifier stability. It may be in your best interest to try and use a more stable amplifier if you can take the hit in bandwidth.
Regards,
Sorry for the delay in reply.
1. It seems that the first stage LMH6629 TIA is a bit undercompensated which is why you might be seeing oscillations in the output waveform. I would recommend you to increase the feedback capacitor in the first stage to 500fF (or higher to 1.2pF) and see if the oscillations go away.
2. Most high speed op-amps (LMH6629 is no different) tend to oscillate when the feedback resistor is high unless they are compensated otherwise using a feedback cap. I noticed that on the 2nd stage the Rf value is 9.5k, which might be the second source of oscillation. I would recommend to make that as 500-ohms and subsequently the Rg as 50-ohms.
3. I would recommend the C4 cap to be reduced from 100pF to 10pF in-order to get more BW out of the cascaded stages.
The AC response below for the above suggestions in TINA-TI look to be good with no apparent peaking, and should indicate the system is stable. I have attached the TINA-TI model for the same.
Best Regards,
Rohit
Hi Ali,
I don't think I have the bootstrap in my model, because I was assuming that you were seeing oscillations without the bootstrap?
Also, for the bootstrap to work properly, you would need the BW in the bootstrap amplifier to be at-least 10x that of the first stage TIA BW. I don't think you have correctly configured the LMH6629 bootstrap op-amp in the figures I am seeing, because the device cannot support unity gain configuration. I think it would better if you switch to OPA656 which can support unity gain operation and has FET inputs. Unity gain buffer amplifiers such as the LMH6559 or BUF602 are also good choices for bootstrapping across the photo-diode cap and LMH6629 TIA gain stage inverting input.
Best Regards,
Rohit
Hi Ali,
What is the issue you are seeing with the bootstrap? Is it oscillations? You could try to increase the value of Rf and Cf and see if the TIA is stable as shown below.
Also, is there a reason as to why you absolutely need the bootstrap? I understand that you want to reduce the photodiode (PD) capacitance, but it comes with the added risk of instability across the TIA loop as well as the bootstrap loop. From the OPA300 datasheet page 8, you can see the output impedance for G = 1 starts to increase at fairly low frequencies ~100kHz with 20dB/decade. It is possible that the issue you are seeing is because of this increase in output impedance where the bootstrap loop is unable to keep the PD cap low at high frequencies. That's the reason for my recommendation of a faster buffer such as the LMH6559 or the BUF602.
The other thing is that the problem you are trying to solve can be achieved without using a bootstrap as well. I have attached a schematic below of the LMH6629 achieving 100MHz BW without using bootstrap. If you looking for even higher transimpedance gain than 1.5k-ohms, then I would suggest looking at the OPA857 which should give ~105MHz BW with 20k TIA gain.
Best Regards,
Rohit
1. LMH6629 with bootstrap:
2. LMH6629 without bootstrap (100MHz BW):
Hi,
My apologies for the delayed reply. I would remove the 100pF capacitor on the non-inverting input as that is likely causing the oscillation on the second stage.
Regards,