Dear;
When I use split power supply of LMH3401, and I wonder why the output is not correct. But single power supply has no problem. Please help to check. Thank you very much.
Best regards
Kailyn
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear;
When I use split power supply of LMH3401, and I wonder why the output is not correct. But single power supply has no problem. Please help to check. Thank you very much.
Best regards
Kailyn
Dear Loren and Sean,
Thank you very much for your reply, and I changed the PD pin to VEE before and found that it could work normally, but the datasheet
describes that PD<0.9V would be active, so I need confirm either the model or the datasheet has something wrong. Now I understand.
Thanks again.
Best regards
Kailyn
Hello Kailyn,
You have identified a weakness in the model. The LMH3401 device has a ground pin. The PD pin threshold is 0.9V above the voltage you apply to the ground pin. The model does not have this pin, so the PD pin is referenced to the Vee pin instead.
This amplifier is somewhat unique as most FDA amplifiers have no ground pin. What is also unique is that the ground pin has no function with regard to the signal path, it is a digital reference only, so we did not think it was a big issue to leave it out from the model.
I hope this answers your questions. I will get an email if you post additional questions to this thread so feel free to post any additional questions.
Regards,
Loren