This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

opa2673: opa2673

Part Number: OPA2673

I am using the OPA2673 as a buffer to drive a large capacitor (10nF) at high speed (100ns). The peak charging current is 600mW but the peak power is about 5W for 10ns. can I exceed the amplifiers power specs for low duty factor pulses?

 

  • Hi Paul,

    Sorry for missing this post.

    I think you might run into thermal issues with the OPA2673 if the amplifier power specs are exceeded. Do you know whether the junction temperature (Tj) of the part could go beyond 150'C while operating the device in low duty cycle pulses with 10nF cap? Also, lower duty cycle of the pulses often results in the part dissipating more heat for longer time compared to the short duty cycle pulses. I would recommend that you take a look at the Thermal Analysis section in the device datasheet to understand a bit more about any thermal issues you might encounter.

    Best Regards,
    Rohit
  • Rohit,

    Thanks for your reply. The opamp is nun at low average power levels so the junction temperatures would be well below operating limits (<80C). The data set does not give any time dependent information e.g. thermal time constants. Is it ok to assume that the thermal time constants are much greater than 1us? If that is the case the temperature rise during each pulse will be small and there will be time for the junction to cool down between pulses. Thats why I think it will be ok to exceed the internal 2W power dissipation limit for short times ~20 ns. However I am not very confident my assumptions are correct so any further insight would be welcome.

    Paul

  • Paul,

    You are right that the thermal time constants on the device are much greater than 1us. If you are running pulses for short times of ~20ns which allows the junction to cool down in-between pulses, then I think it should be ok to exceed the internal 2W power dissipation intermittently.

    Best Regards,
    Rohit
  • Thanks Rohit,

    If you know of any publication (especially by TI) relevant to this topic could you please send me a reference?

    Paul
  • Hi Paul,

    I dont think I have a relevant TI publication on this topic, but it might be possible for you to look into this app note for further information while driving a capacitive load.

    www.apexanalog.com/.../an25u.pdf

    Best Regards,
    Rohit