• Resolved

OPA356-Q1: Cable driver

Part Number: OPA356-Q1

Hi

Our customer are considering that this device can drive coaxial cable at the following input conditions.

- Fin=125MHz,

- Vin_pp=1Vpp @Vdd=3.3V

- Vcm=+1.5V (+/-0.5V=1Vpp)

If it is not possible to use this device at the above condition for cable driver, please give us some other device that you recommend.

(We are considering OPA355 and OPA354 as well.)

Regards,

Koji Hamamoto