DLP Using THS7347 +AFE1000+DDP4421,When VGA Input,stripes will appear when the blue background color is displayed. The digital 、analog power & GND is not separated. When HDMI Input HDMI input does not appear.
In the previous version Use combination of multiple boards And Use the same schematics and software., there was no such stripes when blue background color is displayed .